Reply
Member
PaulNM
Posts: 2
0

Second harddrive in laptop



I purchased a Satellite P770 recently.  One of the reasons I went with the one I did was because it is capable of having a second internal harddrive.  I didn't order it with a second drive because I already have a 500GB drive, and was planning to put in a 1TB later anyway (Toshiba didn't have 1TB drives as an option.).

 

I just discovered that while there is an empty bay, there is no sata port to connect a second harddrive to.  It looks like there's a place where a small board would be mounted, and the sata port the 1st harddrive is connected to also has a ribbon cable connector next to it. 

 

I couldn't find anything on the Toshiba site, does anyone know where can I get the parts I need (second sata port board and harddrive caddy)?  

Super Advisor
brad
Posts: 1,052
0

Re: Second harddrive in laptop

Which model P770 do you have?

 

Also, what's the part number on the sticker on the bottom of the computer?

Member
PaulNM
Posts: 2
0

Re: Second harddrive in laptop

Hi brad, sorry it took so long to reply.

 

It's a Sattellite P770, that's the only thing on the sticker relating to model.

The part number is PSBY3U-0ED026 with <es5.0> on the end.

 

 

Member
ragpicker
Posts: 1
0

Re: Second harddrive in laptop

I imagine by now you found your answer.  If not, the circuit board is available at:

 

http://www.notebooksolutions.ca/zc/toshiba-original-circuit-board-2nd-hdd-conn-ts47437-49764.html