usb power exceeded port when external dvd writer plugged in

Reply
Member
Posts: 2

usb power exceeded port when external dvd writer plugged in

After plugging in external dvd writer, power surge window pops up and tells to disconnect. Says it requires to much power from the usb port. How can I fix problem so I can use the writer? Laptop is a Toshiba Satellite P25-S607, MCE with 2.8 and 1 gig memory. DVD writer is brand new samsung SE-S084 external unit. Any answers?? thanks
Posts: 48,223
Kudos: 9,195
Solutions: 3,263
Registered: ‎12-04-2008

Re: usb power exceeded port when external dvd writer plugged in

 

Satellite P25-S607 

 


How can I fix problem so I can use the writer?

You would need to purchase a powered USB hub. The power is supplied by plugging into your wall receptacle. These are examples.

 

   USB 2.0 4-Port Mini Hub With AC Power

 

   CyberPower USB Hub 7-Port 2.0 with AC Adapter and Flash Drive

-Jerry
Channel 9
Member
Posts: 2

Re: usb power exceeded port when external dvd writer plugged in

Thanks Jerry for the info. It is greatly appreciated. Now I am off to purchase and then let the burning begin.

         

Posts: 48,223
Kudos: 9,195
Solutions: 3,263
Registered: ‎12-04-2008

Re: usb power exceeded port when external dvd writer plugged in

You're welcome. Good luck!

-Jerry
Channel 9