Toshiba Satellite battery charges fast and dies fast

Reply
Member
Posts: 1

Toshiba Satellite battery charges fast and dies fast

Hello Smiley Happy 

 

I have had my laptop for almost a year now and it always runned for about 2h 30 min, recently it had a problem. The laptop was very dirty from the inside so it shut down itself. Took it to a local repair shop and it's brand new now. Just that I've noticed the battery dies VERY fast, and when I re-charge it within minutes it increases from a 42% to a 45% while I finished editing this paragraph . I'm not sure what to do I'm deleting some games and stuff I don't use so it's faster but the battery dies too fast and charges too fast. 

 

PLEASE HELP I'm in finals!!

 

Thanks!

Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: Toshiba Satellite battery charges fast and dies fast

Try the suggestions in this article.

 

Battery not charging, not being recognized, or losing charge

- Peter