Toshiba Satellite S50-A-10P draining power when shut down

Reply
Member
Posts: 8

Toshiba Satellite S50-A-10P draining power when shut down

Hey, my Toshiba Satellite S50-A-10P is draining power when shut down, if I don't use it for like 2 weeks the battery would be dead (0%), even though it was fully charged when I shut it down (I don't have that USB power thing enabled that uses it when it's shut down), anybody know why does this happen? Also the only way to remove the battery is to unscrew the case bolts?

 

Thanks!

Posts: 21,713
Topics: 70
Kudos: 832
Solutions: 482
Registered: ‎10-04-2011

Re: Toshiba Satellite S50-A-10P draining power when shut down

[ Edited ]

That doesn't appear to be a US model, and this is the forums for Toshiba USA. You may want to contact Toshiba in your region. If it's a European model, you could check the Toshiba Europe forums.

- Peter