Reply
Member
Posts: 5

Toshiba Satellite A105 battery charging problem

[ Edited ]

Today I got Toshiba Satellite A105-S2712 for repair with the battery charging problem. It is a new model and we do not have a lot of experience with these laptops. The customer complained that the laptop will not charge the battery when it is plugged into the AC outlet.

The laptop failure symptoms:

The laptop will not turn on when I try to start it from the laptop battery. When the laptop is turned off and plugged into the AC outlet the battery charge LED doesn’t light up. I know that the battery is not charged and the LED should light up when I plug the laptop into the AC outlet. The laptop starts fine when it is plugged. When I move the mouse over the Toshiba Power Icon in the lower right corner, the balloon will pop up and there is a line in there: Battery Remaining: N/A.

The problem repair procedure:

You can easily fix the problem just by updating the BIOS. Toshiba says that the BIOS version should be at least v1.30. So, go to Toshiba website and click on Downloads. Select your laptop model and find any downloads for the BIOS. In the BIOS change history you will see the description of changes.

After I updated the BIOS, the Toshiba Laptop Battery  charging problem disappeared.

 

 

[ admin edit to remove commercial links ]

Member
Posts: 2

Re: Toshiba Satellite A105 battery charging problem

I tried updating the BIOS (have had computer since 2006 and done no updates, so was sure this would fix the problem). It says that I already have the latest version of the BIOS update, though I am still experiencing the battery charging problems. It won't charge at all, and will only work if it's plugged in. Even then, it's iffy because just moving the laptop can cause it to shut down.