Re: Satellite Battery icon reads "no battery detected"

Reply
nm
Member
Posts: 1

Satellite Battery icon reads "no battery detected"

What is wrong with my battery? The battery light is still showing  green....

Super Advisor
Posts: 4,069

Re: Satellite Battery icon reads "no battery detected"

First, try a proper system reset. Power off the laptop, unplug the AC from the unit, remove the battery, press and hold down the power button for 30 seconds, replace the battery and AC, power on, when you see the Toshiba logo, press the 'F2' key to enter the BIOS Setup, in setup press 'F9' to load setup defaults, press 'F10' to save and exit, and then to boot into Windows.

 

Then, try resetting the power plans to the default. Enter this at an elevated command prompt.

 

   powercfg -restoredefaultschemes

 

 

If you need to post back here, we need your full model number, like Satellite L740-ST6N01, and the Windows version you're running like Windows 7 64bit.

 

Please let us know what happens. Good luck.

 

Mike

 

Highlighted
Member
Posts: 2

Re: Satellite Battery icon reads "no battery detected"

This worked for me!  

The first thing you recommended: 

"First, try a proper system reset. Power off the laptop, unplug the AC from the unit, remove the battery, press and hold down the power button for 30 seconds, replace the battery and AC, power on, when you see the Toshiba logo, press the 'F2' key to enter the BIOS Setup, in setup press 'F9' to load setup defaults, press 'F10' to save and exit, and then to boot into Windows.
 

I had same message "no battery detected". When i unplugged the power cord, my computer still worked, but said "unknown remaining." I did what you suggested several hours ago and it's working fine ever since.  (I didn't have to do the elevated command prompt...)

thank you!!!!!

 

Toshiba Satellite L755-S5153.

Super Advisor
Posts: 4,069

Re: Satellite Battery icon reads "no battery detected"

Thanks for lettting us know tagfin. We really appreciate it when people update us on the results of our advice.

 

Mike

Member
Posts: 1

Re: Satellite Battery icon reads "no battery detected"

Hi - I now have this problem on a Portege Z830 (ultrabook).  To remove the battery to do a hard reset I have to open the entire computer.  Is it necessary to remove the battery?

Member
Posts: 1

Re: Satellite Battery icon reads "no battery detected"

I read and tried miker643's recommended "fix" to this but to no avail.  On my Satellite U505-S2970 I just replaced the two 2GB RAM modules with two 4GB RAM modules (after turning power off, disconnecting power and removing battery).  The system started up fine after I replaced the battery and plugged the power in, but the battery light (on the front) never came on and I got the dreaded "no battery detected" message on the system tray icon.

 

After looking up the problem on this forum, I tried it - and even did the DOS commend - in the DOS window, but nothing helped.

 

Suggestions?

Thanks.

Member
Posts: 1

Re: Satellite Battery icon reads "no battery detected"

Hello,

 

that fix did not work for me.

 

OS : Windows 7 home editon
 on Satellite L655-s5156

Member
Posts: 1

Re: Satellite Battery icon reads "no battery detected"

my satellite U405D-S2852, windows 7 Ultimate is telling me No battery dictated, but I charges and switches off at will without notice. please I need your, thanks
Member
Posts: 1

Re: Satellite Battery icon reads "no battery detected"

i left my laptop untouched for two days and now it is showing no battery detected.it was working fine before i left. i tried uninstalling the Microsoft ACPI Compliant Control Method Battery suggested in this forum but it is still showing the same. my laptop is satellite c850-x0110, OS windows 8.1 please help

Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: Satellite Battery icon reads "no battery detected"

That doesn't appear to be a US model, and this is the forums for Toshiba USA. You may want to contact Toshiba in your region.
 
- Peter
Member
Posts: 3

Re: Satellite Battery icon reads "no battery detected"

[ Edited ]

Hi Peter:

I have an old Toshiba Satellite M505-s4972 and I am having the same problem.  It just started after I got my computer back from TSA-LAX. (I left it at the security check point)

 

I did restore system sets from f2 set up; and ran the elevated command powercfg -restoredefaultschemes.

 

I also read your article and uninstalled the microsoft ACPI compliant control driver and reinstalled.

 

The battery is after market that I bought in 4/2012 to replace the original. Is replacing the battery a fix?

 

Any suggestions?

Administrator Administrator
Administrator
Posts: 2,329

Re: Satellite Battery icon reads "no battery detected"

Hi Michael,

 

Peter is on a well-deserved vacation for a couple of days so I didn't want you to wait until he's back.

 

Considering what you've already tried, it does seem likely that you're experiencing a battery problem. You've probably already done this, but I recommend removing & reinstalling the battery to reseat the contacts.

 

Does the laptop work fine with external power connected?

 

Jim

 

Member
Posts: 3

Re: Satellite Battery icon reads "no battery detected"

Hi Jim:

 

Thank you for jumping in for Peter.  I have followed all the steps set out by Peter, including brushing the contacts. The laptop works fine with just the AC plug in, unless of course the AC comes out accidentally then we have a small crash.

 

Let me know if there is a next step for me to follow.

 

best

 

michael

Administrator Administrator
Administrator
Posts: 2,329

Re: Satellite Battery icon reads "no battery detected"

Glad to help, Michael, if I can.  Smiley Happy 

 

I'd say this all points to a fairly high likelihood that the battery is indeed the problem. I can't guarantee it since an issue with the charging system could present the same symptom. But a battery replacement is much easier and less expensive than a visit to a repair shop for a more definite hands-on diagnosis.

 

If it was my system I'd try replacing the battery next...

 

Jim

Member
Posts: 3

Re: Satellite Battery icon reads "no battery detected"

Hi Jim

 

Thanks I will replace battery and let you know if that is a fix.

 

best

 

michael

Member
Posts: 1

Re: Satellite Battery icon reads "no battery detected"

Didnt work for me.  I bought a new battery thinking it was a battery issue.  But I still can't use my computer without the AC plugged in.  Reformat doesnt work either.

 

Toshiba Satellite L300

Windows Vista 32bit

Member
Posts: 1

Re: Satellite Battery icon reads "no battery detected"

Satellite Battery icon reads "no battery detected" satellite pro P300-28L I tried what you said but it didn't work NOTE : I had a new battery
Posts: 21,719
Topics: 70
Kudos: 852
Solutions: 483
Registered: ‎10-04-2011

Re: Satellite Battery icon reads "no battery detected"

You could try the suggestions in this article:

 

Resolving battery and power issues

- Peter
Member
Posts: 2

Re: Satellite Battery icon reads "no battery detected"

So I upgraded my Toshiba L655- S5117 from Windows 7 to Windows 10.  The install went smoothly but now my battery icon is saying "No battery detected"  The laptop is still working fine and charges with no issues but I can't seem to figure out now to resolve that issue.  I don't want to do the system reset because I am afriad it will remove my Windows 10 update.  

 

What should I do?