Laptop won't turn on without the charger connected

Reply
Member
Posts: 1

Laptop won't turn on without the charger connected

When I unplug my charger from the laptop it completely goes off, and when I try to turn it back on without the charger, it won't turn back on. 

Posts: 21,713
Topics: 70
Kudos: 821
Solutions: 482
Registered: ‎10-04-2011

Re: Laptop won't turn on without the charger connected

Can you check the laptop's full model and part numbers from the label on the bottom? Don't include the serial number.

- Peter
Member
Posts: 2

Re: Laptop won't turn on without the charger connected

I am having the same problem and also mine will not charge any higher than 37% Satellite C55-A5300.

Please help

Member
Posts: 2

Re: Laptop won't turn on without the charger connected

Satellite C55-A5300  part # PSCFEU-OOMOOG  Will not charge or turn on without being plugged in.

 

Posts: 21,713
Topics: 70
Kudos: 821
Solutions: 482
Registered: ‎10-04-2011

Re: Laptop won't turn on without the charger connected

I believe you have a problem with your battery. You can use the Troubleshooting Assistant. If it concludes that the problem is the battery, it'll set up a battery swap. You could select the symptom dealing with a battery that won't charge. If you continue to tell it that your battery won't charge, it'll lead you to the conclusion that it needs to be replaced.

- Peter
Posts: 21,713
Topics: 70
Kudos: 821
Solutions: 482
Registered: ‎10-04-2011

Re: Laptop won't turn on without the charger connected

This thread has been moved to another message board. Click the link to jump to its new location.

Member
Posts: 1

Re: Laptop won't turn on without the charger connected

Laptop won't turn on without the charger connected 

this laptop is like few months old..  what do i do?     C55-A5300

Posts: 4,848
Topics: 57
Kudos: 1,616
Solutions: 377
Registered: ‎05-03-2009

Re: Laptop won't turn on without the charger connected

Probably a bad battery.  Call Tech Support at 1-800-457-7777 for a replacement.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit