Reply
Member
Posts: 3

DC Power Jack toshiba satellite a135-s4666

I need to replace my dc power jack for my toshiba satellite a135-s4666. I looked at ebay and i'm sure if these two are different or not they say they both work but they look slightly different which one is the right one for me?

http://cgi.ebay.com/DC-Power-Jack-Repair-Toshiba-Satellite-A135-S4666_W0QQitemZ370052469479QQcmdZVie...

or

http://cgi.ebay.com/AC-DC-JACK-POWER-IN-PORT-TOSHIBA-SATELLITE-A135-S4666_W0QQitemZ220408130991QQcmd...

 

 

Thanks

Member
Posts: 3

Re: DC Power Jack toshiba satellite a135-s4666

Member
Posts: 3

Re: DC Power Jack toshiba satellite a135-s4666

[ Edited ]

So no ideas yet?

I just can't figure out what to do lol cause I'm pretty sure I need to replace the DC power jack but from the tutorial i was following(link at second post) it was at a different place than mine(I have pictures of mine on the second post) so I'm not sure what to do

Regular Advisor
Posts: 3,300

Re: DC Power Jack toshiba satellite a135-s4666

Your original post- the second link is more feasible.  To be sure call Toshiba(800) 457-7777 to learn if a part is available for your repair.  Look here:  http://www.sparepartswarehouse.com/Toshiba,Satellite,A135,PSAD0U-0N600N,Laptop,Parts.aspx 

Member
Posts: 5

Re: DC Power Jack toshiba satellite a135-s4666

I don't know if this will help you, but I found this while looking for parts to repair

my old m45-s165. They may have something for yours..

 

Toshiba Laptop Parts

Regular Advisor
Posts: 3,300

Re: DC Power Jack toshiba satellite a135-s4666

Thanks for posting this interesting parts store website rmgs45.

Member
Posts: 10

Re: DC Power Jack toshiba satellite a135-s4666

Go here:

 

http://www.insidemylaptop.com/repair-damaged-power-jack-toshiba-satellite-l305-l355-laptops/

 

My jack broke and I picked up the jack at radio shack for $3. It's metal and tightens securely from the inside and outside of the case so it won't break off or get pushed in like the old jack. Hope this helps

 

Cheers!