1905-S277

Reply
Member
Posts: 5

1905-S277

I seem to be having a converter/charging problem but am not sure.   My converter seems to be working however, when plugged in the battery light on the front of the machine will sometimes stay on, sometimes flash and sometimes go out completely.  When I look at the icon in the taskbar it will show "Full power remaining: 6% On AC Power".  It's always sain 100% On AC Power.  When I look at the power options it will tell me that I'm on AC power but it will also show my battery as discharging.  Then the maching shuts off regardless if I'm plugged into an outlet or not.  How do I determine the cause of this and possible solution?  Thanks.