Volume Control

Reply
Member
Posts: 7

Volume Control

Hello.

 

My laptop volume speakers are not loud enough. I have it on the max levels and still I'm having to lean forward to hear what I'm listening too. So is there a way that I can make my laptop speakers Louder ?

 

Hope so..

 

Thanks

 


Member
Posts: 7

Re: Volume Control

Hello ? I'm still waiting on a reply....

Super Advisor
Posts: 4,069

Re: Volume Control

Short answer is no, you can't make your built in speakers louder.

 

Plus you don't give your full model number, nor it's part/product number, nor the version of Windows and its bitness that you are using.

 

So, it's very difficult to offer any other advice, except to buy a set of external speakers, with their own power source, that will give you the volume you are looking for.

 

Mike

Member
Posts: 7

Re: Volume Control

[ Edited ]

It's ok. I just overclocked myToshiba Qosmio Laptop / Intel® Core™ i5 Processor 2.53 Ghz to 3.00 Ghz and I glitched my laptop speakers to a 100 %. The dafault settings was clocked at 65 %. 

 

Thank goodness for overclock forums.

 

Cheerio Smiley Very Happy

 

Oh and btw, if the short answer was no, then why did you waste your asking me for my numbers and stuff, if the answer would still be no ? lol FAIL

Super Advisor
Posts: 4,069

Re: Volume Control

Your last name isn't Paulsen by any chance, is it?

 

Mike