Toshiba satellite U305-s5077 with Realtek ALC268 - No sound, but sometimes.

Reply
Member
Posts: 2

Toshiba satellite U305-s5077 with Realtek ALC268 - No sound, but sometimes.

Hi, i have a Toshiba satellite U305-s5077 with Realtek ALC268 audio board. Windows 7 installed.

PROBLEM : Sometimes, only sometimes, i have audio on my laptop, maybe in the afternoon but non in the evening.

 

1 - When i have audio I can see the driver and i upgrade it to the last driver (Image1 attached)
Drivers downloaded from: http://www.realtek.cz/realtek-download.php?realtek=ALC268&system=5

 

2 - But when i have not audio, no driver (Image2 attached)

 

I apreciate any help.
Thanks

  


Posts: 21,713
Topics: 70
Kudos: 824
Solutions: 482
Registered: ‎10-04-2011

Re: Toshiba satellite U305-s5077 with Realtek ALC268 - No sound, but sometimes.

Have you tried reinstalling the latest sound driver offered by Toshiba?

 

Realtek Audio Driver for Windows 7 (32/64)(v6.0.1.5854; 09-04-2009; 36.27M)

- Peter
Member
Posts: 2

Re: Toshiba satellite U305-s5077 with Realtek ALC268 - No sound, but sometimes.

 

Hi Peter, yes, that was the first try. But this driver is date 2009 (see attachment), so I looked for a newer driver in Realtek. But don't work either.

 

thanks.


Posts: 21,713
Topics: 70
Kudos: 824
Solutions: 482
Registered: ‎10-04-2011

Re: Toshiba satellite U305-s5077 with Realtek ALC268 - No sound, but sometimes.

Did this just start happening?

 

Try using System Restore to restore a previous restore point from before this became an issue.

- Peter