10-23-2011 04:43 PM
I have windows 7 on may toshiba satellite
10-24-2011 07:54 AM - edited 10-24-2011 08:05 AM
I found a problem....
My network adapters are a problem
they causes interference
when I disable them sound is normal.
But new network adapter drivers did not help
01-23-2012 07:30 PM
hey I checked this and you're right about the network adapters, have you found a way to fix it?
01-24-2012 10:39 AM
02-25-2012 11:23 PM
I am having the exact same problem, and I like to use Pandora so I don't want to have to stop my wi-fi, etc. Has anyone found a fix yet?
02-25-2012 11:44 PM
I found the answer thanks to another blog post--it's the Conexant driver that is the problem. Go to your Control Panel, open up Programs and Features, and Uninstall the Conexant driver. Reboot your laptop, and the Microsoft sound driver will load instead. Problem fixed! Yay
02-29-2012 08:30 AM
I've been having the same problem with my Satellite. How does the Microsoft sound driver load? does it do it automatically. I've go a Satellite L655-5083, what is your version. It's running Windows 7 with the Intel Pentium.
05-19-2012 05:58 AM
I updated the antheros Network adapter driver. It didnt work.
I updated the Realtek wireless Lan driver. It didnt work.
Finally, I disabled antheros Network adapter.
And it worked!
Toshiba still didnt provide solution for this problem.
08-07-2012 05:42 AM
Toshiba have now provided a solution, you can update the atheros driver here:
http://aps2.toshiba-tro.de/wlan/?page=downloads
and it fixes the problem! Much happier!!
09-27-2012 01:32 PM
Hello. Not sure if this is the same issue, but I recently discovered I was having a real problem with my new laptop. Just got it one week ago. I like it, except that the audio recorder doesn't work. I use goldwave, an audio editor/processor/recorder, and have for years, on laptops as far back as the 90s
but with this laptop, it says it can't record audio. I'm at a loss, because I've never had this problem. At first, I was able to record from the microphone, but when I told it to record what was playing on the computer, it wouldn't let me, it said it wasn't able to.... Is there something I have to download?
Any help VERY appreciated, guys!!!
09-27-2012 01:51 PM
not sure if this helps, but i tried to troubleshoot, and found this message:
MME (waveIn):
No recording devices detected!
10-12-2012 06:29 AM
so no one has any idea? what is this toshiba forum used for, anyway? they sold me on how awesome the sound was supposed be , and then it doesnt work right and i cant seem to catch a break... hmm..
05-15-2013 04:49 AM
I just want to say... you rock! ![]()
I couldn't hear to music or videos without that random-annoying sound. I was about to contact consumer-support to have it fixed before my two-year guarantee expires, but thanks to the solution you've provided in this thread now it's working fine.
I reinstalled the audio drivers several times and it didn't solved the problem. I couldn't figure out that the problem was caused by the wireless-lan atheros driver. I installed the atheros driver provided by Toshiba: http://aps2.toshiba-tro.de/wlan/?page=downloads and now it works perfectly.
Thank you very much![]()
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.