Protege M600 Sound Problem

Reply
Member
Posts: 1

Protege M600 Sound Problem

I have brought the Toshiba Protege M600 in HK and re-install it with winXP, but the sound didn't work now, any drive update that can made it works again ????  Tks~~

Posts: 46,819
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Protege M600 Sound Problem

Which Portege M600? What's the part number?

 

For example, the part number for model M600-E360 is PPM60L-013009.

-Jerry
Channel 9
Occasional Contributor
Posts: 15

Re: Protege M600 Sound Problem

hi,

 

i also have same problem with portege m600 i installed win7 , xp but i din't got my audio there i installed latest drivers latest bios but nothing worked so plz help....

 

 

my part no. is - PPM60L-02D00W

 

 

PLZ HELP ME OUTSmiley Sad

Occasional Contributor
Posts: 15

Re: Protege M600 Sound Problem

PLZ HELP ME OUT SOONSmiley Sad

Posts: 46,819
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Protege M600 Sound Problem

 

Portege M600 (PPM60L-02D00W)

 

An Asian machine. Have you tired this driver?

 

   Realtek Audio Driver for Windows7, 6.0.1.5898

   065913_02.01.35.TC70050200A.exe

 

 It's for 32-bit Windows 7 only. I don't see one for 64-bit Windows 7.

-Jerry
Channel 9
Occasional Contributor
Posts: 15

Re: Protege M600 Sound Problem

just now i'm using windows xp  but when i was using windows 7 32 bit i tried all the latest driver from 

 


http://support.toshiba-tie.co.jp/windows7/download/PORTEGE_M600_32_sp.htm but nothing happened i had same problem...

 

i updated bios ,tried with chipset utility , used various audio driver but still no audio...

there is no icon in task bar ...Smiley Sad

Occasional Contributor
Posts: 15

Re: Protege M600 Sound Problem

this is my device manager..
Occasional Contributor
Posts: 15

Re: Protege M600 Sound Problem

in my device manager there comes question mark on Modem Device on High Definition Audio Bus...

Posts: 46,819
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Protege M600 Sound Problem

Have you installed the modem driver?

 

Mystery to me now which version of Windows you want to talk about.

-Jerry
Channel 9
Occasional Contributor
Posts: 15

Re: Protege M600 Sound Problem

Which modem driver? i can't find it out,

i use xp version 5.1...

Posts: 46,819
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Protege M600 Sound Problem

Occasional Contributor
Posts: 15

Re: Protege M600 Sound Problem

As u said to install modem driver, i installed toshioba modem driver for xp also but sound still not coming plz help me out...

Posts: 46,819
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Protege M600 Sound Problem

You need to decide which version of Windows you want.   

-Jerry
Channel 9
Occasional Contributor
Posts: 15

Re: Protege M600 Sound Problem

Smiley SadSo isn't there any sollution for my portege m600 from your side now what should i do of it i have installed all the drivers updted bios in xp as well as windows 7...

 

 

But still audio problem is there ....Smiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley Sad

Posts: 46,819
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Protege M600 Sound Problem

So you can't decide which Windows? Let's talk about Windows XP.

 

The order of installation matters.

-Jerry
Channel 9
Occasional Contributor
Posts: 15

Re: Protege M600 Sound Problem

i din;t understand i'm using xp currently...

 

you sugest me to use which version of windows ill use it xp or win7...Smiley Happy

Posts: 46,819
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Protege M600 Sound Problem

Let's start all over again with a fresh install of Windows XP? Reformat the drive and install it.

 

Which version do you have? Professional? With which service pack preinstalled?

 

After that, get the Toshiba drivers and utilities for a Portege M600 here.

 

Install the Intel chipset utility followed by the display driver (downloads in three parts) prior to any other driver. With a little luck, that will solve the audio problem.

 

Install the Toshiba hotkey utility before other Toshiba utilities.

-Jerry
Channel 9
Occasional Contributor
Posts: 15

Re: Protege M600 Sound Problem

[ Edited ]

as you told to reformat my M600 with xp i did it ...

 

 

but nothing worked on it 

 

i installed the drivers as you told but nothing worked my laptop still have no sound Smiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley SadSmiley Sad

Posts: 46,819
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Protege M600 Sound Problem

Sorry, I can't help more. Maybe the hardware is defunct.

-Jerry
Channel 9
Occasional Contributor
Posts: 15

Re: Protege M600 Sound Problem

[ Edited ]

can you help if i use win7?

 

and is there audio that should be enabled in bios ?

 

i searched but i didn' foundSmiley Mad