Laptop SOUND fades when VOLUME control keys used

Reply
Member
Posts: 1

Laptop SOUND fades when VOLUME control keys used

[ Edited ]

Why does the sound on my laptop fade momentarily when I use the volume keys "-" "+" to adjust up and down volume.  I have to wait for the sound to come back, which takes about 3 - 4 seconds to hear what the newly adjusted volume is.  It makes it difficult to control the volume because I can't hear the change in loudness until the sound comes back.  Can this "feature" be changed.  I there some purpose to why the sound fades? 

Posts: 21,713
Topics: 70
Kudos: 832
Solutions: 482
Registered: ‎10-04-2011

Re: Laptop SOUND fades when VOLUME control keys used

Can you check the laptop's full model and part numbers from the label on the bottom? Don't include the serial number.

- Peter