Reply
Member
solomon40
Posts: 1
0

L755 low volume

I have my speakers cranked on high and I can barely hear anything I play. I updated the drivers for the audio but its still the same. Wondering if I am stuck with it this way.

Moderator
Peter
Posts: 10,533
0

Re: L755 low volume

In Windows 7, you can set the master volume independently of the volume of individual applications. Right-click the speaker icon in the notification center (near the clock) and select "Open Volume Mixer." The leftmost pane is the master volume. To the right are individual applications. Make sure you turn the volume up for the application and the master volume!

 

You could also right-click the speaker icon and select "Playback Devices." Select your speakers and click "Properties." Try changing the settings in the "Enhancements" tab to see if that helps!

- Peter
Member
bob8
Posts: 3
0

Re: L755 low volume

I have the same complaint. The sound is simply too low regardless of source or settings. I have an old Dell that has 5 times the volume. Toshiba should care enough to fix this.