Headphones in, audio out both laptop and headphones

Reply
Member
Posts: 4
Accepted Solution

Headphones in, audio out both laptop and headphones

Is this a coincidence that it happened around the same time or is there an option in the computer to turn off the laptop speakers when the audio input is detected? 

As the subject says, whenever I plug in my headphones, sound comes out from both the laptop speakers AND the headphones. I think this occurred when a bit of the outside ring got chipped off. I have a picture of the audio jack.

 



Accepted Solutions
Super Advisor
Posts: 4,069

Re: Headphones in, audio out both laptop and headphones

Then it would appear that your problem is no coincidence in regard to the headphone jack damage. You can only try to get the Mic, Headphone Jack Board replaced, as it would appear to be no longer capable of sensing when you plug something in.

 

Mike

View solution in original post


All Replies
Super Advisor
Posts: 4,069

Re: Headphones in, audio out both laptop and headphones

[ Edited ]

I think it's coincidence about the chip. Without your headphones  plugged in, try going into Control Panel and see if you have 'Realtek HD Audio Manager' and then click on that. Inside this on the right hand side, above ANALOG, you will see a little folder icon, click on that and put the checkmark on 'Enable auto pop dialog....' and click 'OK'. Then try to plug your headphones in again, and put the checkmark on 'Headphones' and click 'OK'.

 

If you do not have the Realtek HD Audio Manager in Control Panel, then give us your specific model number/name like, Satellite C655-S5047, and your model's Part Number, like PSC08U-00V01E. You can find this info on the Toshiba label on the bottom of your computer. Also, we need your OS version like Windows 7 64bit. You should always give this information everytime you post a problem here.

 

Please let us know what happens, or get back to us with the above information. Good luck.

 

Mike

Member
Posts: 4

Re: Headphones in, audio out both laptop and headphones

Thank you for responding so quickly Smiley Very Happy

 

I did the steps, but when I plugged my headphones back in, the pop-up dialogue didn't well, pop up. The headphones still plugged in as usual and i heard sounds from both the laptop and the headphones (I DID press okay on the screen to make sure the settings saved before I plugged in the headphones).

 

Here is my computer information:

Satellite M645-S4070

Part No.: PSMPBU-00R01R <ES5.0>

I am running a Windows 7 64-bit.

Super Advisor
Posts: 4,069

Re: Headphones in, audio out both laptop and headphones

Satellite M645-S4070

 

 

Let's try reinstalling your sound driver that controls all that. Also, make sure you push headphone jack in all the way. Download this file to your desktop and double click on it to install.

 

Realtek Audio Driver

 

 

Please let us know what happens. Good luck.

 

Mike

Member
Posts: 4

Re: Headphones in, audio out both laptop and headphones

I reinstalled the sound driver and it still acts as it did before (sound out of both headphones and speakers). I also went through the previous steps again, but with no success.

 

One other point that I left out was that when the ring popped out, i pushed my headphone jack in "all the way," which may have hurt some of the inside mechanics.

Super Advisor
Posts: 4,069

Re: Headphones in, audio out both laptop and headphones

Then it would appear that your problem is no coincidence in regard to the headphone jack damage. You can only try to get the Mic, Headphone Jack Board replaced, as it would appear to be no longer capable of sensing when you plug something in.

 

Mike

Member
Posts: 4

Re: Headphones in, audio out both laptop and headphones

All right. Thank you very much for your input and time!

Member
Posts: 1

Re: Headphones in, audio out both laptop and headphones

Hi, I am having the same problem ~ speakers do not turn off when headphones plugged in.  I have a L455D-S5976 and there is not a "Realtek HD Audio Manager" option in the Sounds panel.  I tried to change the "Playback devices" to headphones, however, Speakers are the only option.   What should I do?

 

Thanks!

Kristen

Member
Posts: 1

Re: Headphones in, audio out both laptop and headphones

I did the steps, but when I plugged my headphones back in, the pop-up dialogue didn't well, pop up. The headphones still plugged in as usual and i heard sounds from both the laptop and the headphones (I DID press okay on the screen to make sure the settings saved before I plugged in the headphones)

Member
Posts: 1

Re: Headphones in, audio out both laptop and headphones

Hello, my microphone does not work. Waht can I do?? I have a Toshiba Satellite L755-S5244 Laptop

 

 I do not have the Realtek HD Audio Manager in Control Panel. My OS version is Windows 7 64bit.

 

Thank you

Member
Posts: 1

Re: Headphones in, audio out both laptop and headphones

Thanks Mike, had the same problem and it worked.

Member
Posts: 1

Re: Headphones in, audio out both laptop and headphones

I have a brand new Toshiba L850d satellite and had the same problem and like most was frustrated trying to get the speakers to turn off with the headphones plugged in and then it hit me leave the headphones plugged in and restart the computer and it worked (autodetect? i guess) Listening to tunes and typing hope this helps someone worked for me.      Rock it!

Member
Posts: 1

Re: Headphones in, audio out both laptop and headphones

What is the file for the Realtek HD Audio Manager for my laptop? My information is: Satellite C655D-S5332, Windows 7 64bit, Part number, PSC0YU-03T02D.

Member
Posts: 1

NO SOUND IN SPEAKER OR HEADPHONE

HI, MY LAPTOP IS A M645-S4070 AND NO SOUND NEITHER SPEAKER OR HEADPHONE BUT WHEN I CONNECT THE HEADPHONE I CAN LISTEN A SOUND LIKE A SCRATCH IN THE SPEAKER BUT IT'S RARE THEY SOUND I'D TURN OFF THE LAPTOP WHEN I TURN ON IN THE NEXT DAY THEY BE IN SILENT FOREVER

Member
Posts: 2

Re: Headphones in, audio out both laptop and headphones

there is no option above the analoge icon on windows 8


 

Member
Posts: 2

Re: Headphones in, audio out both laptop and headphones

toshiba pcs are somehow  are not good at sound systems  specialy their earfon plugin slots  and i shuould hv to plug in my earphone not to far inside not far out side zat means inorder to get a correct sound i hav to plugin to the middle and i cant connect to external speakers and get cool sounds

 

Member
Posts: 1

Re: Headphones in, audio out both laptop and headphones

Very frustrating problem, easy solution-- just restart with the headphones in.  Problem fixed!  Thanks a million!