09-26-2011 01:49 PM
Where is Thrive's Windows USB driver for SDK or AppInventor?
I only starting Android development, so I may have my words wrong.
I am developing in Windows 7, and I believe I need a driver to direct connect the PC to the Thrive via a USB cable.
Can someone help me?
Thanks!
09-27-2011 10:09 AM
You have a couple of options. The USB ADB drivers to use are the generic ones that are provided in the Android SDK, but you do have to edit the config file. The easy way is to go to ThriveForums.org or TabletRoms.com and download my easy flash tool. It contains the USA ADB drivers and the edited configuration file.
10-03-2011 01:55 PM
Awe, dale, I was going to say that. ;-) Trying to help out here, noticing there is a major lack of end user support from toshiba on their own forums.
02-26-2012 12:28 AM
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.