Reply
Occasional Contributor
Steerpike
Posts: 10
0

Can someone help me rollback with no fastboot and no service station?

That's the problem in a nutshell.


The update yesterday broke a lot of the tablet. Fastboot is gone. I downloaded the rollback, but it won't work because one of the things that is now broken is service station, so I can't use it. So the tablet is screwed up after the update, and at the same time Toshiba removed the tool I need to fix it.

 

Any thought?

 

Any way to rollback and get fastboot again without service station?

Regular Advisor
austeregrim
Posts: 183
0

Re: Can someone help me rollback with no fastboot and no service station?

Contact Toshiba customer support. They will probably have to repair/replace it for you.

- Signature Starts Now -
I don't work for Toshiba, so please consider my advice Free; like Open Source.
*OH HAIZ! I rooted teh Thrives*
- End Signature -
Regular Advisor
dalepl
Posts: 375

Re: Can someone help me rollback with no fastboot and no service station?

You can download a copy of the downgrad OTA from here:  Official Toshiba HMJ37.31.5.0011 to HMJ37.01.5.0032 Downgrade

 

This is the official file and is signed by Toshiba, so you can install it via recovery.

Paul L. Dale
**********************************************
Thrive Developer - ThriveForums.org