Reply
Member
Mystic_Ninja
Posts: 1
0

Upgrading or switching graphics/video cards on DX735-D3201 All-in-One Desktop

Just a simple question. Can I still change or update graphics or video cards on an all-in-one desktop like the model DX735-D3201?

Regular Contributor
Funky1096
Posts: 58
0

Re: Upgrading or switching graphics/video cards on DX735-D3201 All-in-One Desktop

[ Edited ]

ANYTHING and i repeat ANYTHING with any form of intel hd graphics by toshiba are one of two things: Crap, and they dont come with pci-e expansion slots!

 

So there is no way unless you want to go into complicated soldering techniques then beg toshiba to release a driver to replace intel hd grapics.

 

please so help me if you can find a inexpensive toshiba laptop with a pci-e expansion slot for graphics.

 

I wanted to make that clear to all casual computer buyers.



laptops- ex satillite l755-s5353 inspiron e1505 desktop dimension 400/300