Taking screen shots with the Toshiba Satellite C6550-S5300 laptop computer

Reply
Member
Posts: 1

Taking screen shots with the Toshiba Satellite C6550-S5300 laptop computer

I have the Toshiba Satellite C6550-S5300 laptop computer and I am trying to take a screen shot.  Does anyone know the keys or "F" button to press?  I thought it was CTRL + PRTSC. 

Posts: 4,849
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: Taking screen shots with the Toshiba Satellite C6550-S5300 laptop computer

[ Edited ]

Mark, although you have posted in the All-In-One Computer Forum with an incorrect Model number, I assume you mean C655D-S5300. Press FN+PRTSC for the whole screen and FN+ALT+PRTSC for the active window.  If you are using an external keyboard, substitute CTRL for FN.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Posts: 46,822
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Taking screen shots with the Toshiba Satellite C6550-S5300 laptop computer

 

Satellite C655D-S5300

 

 


I thought it was CTRL + PRTSC. 


Mark, PrtSc alone will copy the screen to your clipboard. Alt + PrtSc will copy just the active window to the clipboard.

 

Then you'll need to paste the picture into an image-compliant application, like Paint (mspaint.exe) or Word (winword.exe), and use Save As on its File menu to create an image file.

You can capture any portion of the screen using the Snipping Tool (snippingtool.exe).

 

   Use Snipping Tool to capture screen shots

 

I have a shortcut to it and have made a keyboard shortcut (Ctrl + Del +S) to bring it up.

-Jerry
Channel 9
Posts: 46,822
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Taking screen shots with the Toshiba Satellite C6550-S5300 laptop computer

CB, you hit the Post button just two minutes before it did. So you get the cigar.

-Jerry
Channel 9
Posts: 4,849
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: Taking screen shots with the Toshiba Satellite C6550-S5300 laptop computer

Just barely!!! BTW, PRTSC alone on the Toshiba keyboard will get you nothing. On the external keyboard, it works your way.

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Posts: 46,822
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Taking screen shots with the Toshiba Satellite C6550-S5300 laptop computer


PRTSC alone on the Toshiba keyboard will get you nothing.


One needs to be smart enough to reach PrtSc. No?

-Jerry
Channel 9
Posts: 4,849
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: Taking screen shots with the Toshiba Satellite C6550-S5300 laptop computer

You lost me, Jerry. 

 

C.B.

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Posts: 46,822
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Taking screen shots with the Toshiba Satellite C6550-S5300 laptop computer

Laptops have many keys with multiple meanings.

 

I'm using a Lenovo with PrtSc and SysRq on the same key. It requires Fn to reach SysRq.

 

Next to me there is a Compaq with Insert and PrtSc on the same key. That one requires Fn to reach PrtSc.

 

The situation is clearly indicated on the key.

 

It's up to the operator to know the difference.

-Jerry
Channel 9
Posts: 4,849
Topics: 57
Kudos: 1,617
Solutions: 377
Registered: ‎05-03-2009

Re: Taking screen shots with the Toshiba Satellite C6550-S5300 laptop computer

[ Edited ]

On my Toshibas, the PRTSC is shared with END above (no idea what that does). HOME (above) and SYSRQ (below) share the key next door. No idea what SYSRQ does. On the external keyboards I have here, Print Screen is a separate key all by itself and, of course, there is no FN key. Whatever happened to standardization?

 

C.B..

C.B.

Toshiba Sat. C75D-B7260 Win 8.1 64 Bit--Toshiba Sat. L775D-S7132 Win 10 Home RTM Upgrade from W7 and Win 10 PRO Insider Preview--Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit--Toshiba Sat. Radius P25W-C2300-4K Win 10 Home 64 Bit
Posts: 46,822
Topics: 83
Kudos: 8,814
Solutions: 3,146
Registered: ‎12-04-2008

Re: Taking screen shots with the Toshiba Satellite C6550-S5300 laptop computer


Whatever happened to standardization?


That's the point. There is no standardization for these keys on laptops. Not even for one OEM. On some of our Compaqs, there's no need to press the Fn key for PrtSc.

 

BTW, the reason it's called Print Screen is that it really did send what's on the screen to the printer. That was prior to the advent of the GUI (Windows).

-Jerry
Channel 9