Reply
Occasional Contributor
curlymixl9
Posts: 13
0
Accepted Solution

Installing Memory on DX730-ST6N03

I have an DX730 which cam with 8 g of memory upgradable to 12 and I have the extra memory stick but when I

open the memory cover there are the A and B slots but I do not see a place for the additional stick,,,What am I doing wrong? or is there something I am missing?

Super Advisor
cbwilsha
Posts: 2,578
0

Re: Installing Memory on DX730-ST6N03

Your User's Guide pretty thoroughly explains how to add memory.  See page 31 of User's Guide.  There are ONLY 2 slots.  If you want to add memory, one of the slots has to be replaced.

 

C.B.

C.B.
Toshiba Sat. L675D-S7016 Win 8 PRO 64 Bit---Toshiba Sat. L775D-S7132 Win 7 PRO SP3 64 Bit which also has Virtual Machine with Win XP SP3---Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit
Occasional Contributor
curlymixl9
Posts: 13
0

Re: Installing Memory on DX730-ST6N03

This model desk top model has 8 installed and it was expandable to 12 unless I misunderstood something.

Super Advisor
cbwilsha
Posts: 2,578
0

Re: Installing Memory on DX730-ST6N03

The specifications for your machine also located here says about Memory--Configured with 8GB (Max 16GB).

 

C.B.

C.B.
Toshiba Sat. L675D-S7016 Win 8 PRO 64 Bit---Toshiba Sat. L775D-S7132 Win 7 PRO SP3 64 Bit which also has Virtual Machine with Win XP SP3---Toshiba Sat. L305-S5921 Win Vista SP2 32 Bit
Regular Contributor
Covered
Posts: 74
0

Re: Installing Memory on DX730-ST6N03

It is not possible to "add" another stick since there are only two slots.  You must remove a 4G stick and insert an 8G stick.