04-06-2012 06:29 PM
I have an DX730 which cam with 8 g of memory upgradable to 12 and I have the extra memory stick but when I
open the memory cover there are the A and B slots but I do not see a place for the additional stick,,,What am I doing wrong? or is there something I am missing?
Solved! Go to Solution.
04-07-2012 07:25 AM
Your User's Guide pretty thoroughly explains how to add memory. See page 31 of User's Guide. There are ONLY 2 slots. If you want to add memory, one of the slots has to be replaced.
C.B.
04-08-2012 02:31 PM
This model desk top model has 8 installed and it was expandable to 12 unless I misunderstood something.
04-08-2012 04:04 PM
The specifications for your machine also located here says about Memory--Configured with 8GB (Max 16GB).
C.B.
04-27-2012 07:37 AM
It is not possible to "add" another stick since there are only two slots. You must remove a 4G stick and insert an 8G stick.
Copyright © 2013 Toshiba America Information Systems, Inc. All rights reserved.